AXIS#.IL.OFFSET

Description

This value is added to the overall current loop feedforward value. A constant current command can be used to compensate for gravity.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A

Range

AXIS#.IL.LIMITN to AXIS#.IL.LIMITP

Default Value

0 A

Data Type

Float

See Also

AXIS#.IL.FF

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.IL.OFFSET 0x500A 0x10 DINT 1000:1 - RW False
AXIS2.IL.OFFSET 0x510A 0x10 DINT 1000:1 - RW False